hello everyone,
im working on bms for which I'm using bq76920. which awsome ic. thank to ti .
ov,uv ,scd,ocd is working fine.
now I'm trying to implement balancing on this ic. but when I start balancing around 890 mA current is displayed. but when I checked across shunt there is no drop across the shunt. what may be the issue.?
also after detecting the short circuit or overcurrent fault, what should be next logic. I'm thinking after short circuit or overcurrent is detected until we disconnect the load MCU won't turn on the MOSFET. is there any other method or logic for this ?. because if we connect this BMS to some circuit and accidentally we short or overcurrent occurs we have to disconnect and connect again.
thank you in advance.