This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LM5175: LM5175 instability with Vin = 9-15Vdc, Vout = 12V, Iout = 10A

Part Number: LM5175
Other Parts Discussed in Thread: LM5176

Tool/software: WEBENCH® Design Tools

We have designed in the Webench a DC-DC converter with Vin = 9 to 15Vdc, Vout = 12Vdc, Iout = 10A.

The controller LM5175 goes to instability at Vin < 10V or Iout > 4A. 

I have found here in the forums three similar cases, but the solution suggested is the migration for the LM5176 controller.

Anyone have solved the problem only with the adjustment of the control components?