Other Parts Discussed in Thread: EV2400, BQSTUDIO
Hi,
I am running into the same issue as Alessandro Berruti. I've got the BQ35100EVM connected to the EV2400. I am also using the SAFT LS 17500 LI-SOCL2 battery but only one bat. After reading this article i also changed the Chem ID to 0x0607. I also used the same steps as Alessandro. My design is right now:
BAT+ | -----------|----------------- | -------- | --|--------- | --- | -- manual Switch -- | --| |
SAFT LS 17500 3,6V | 20 kOhm | 150 Ohm | ||||
BAT- | -----------| | | | | | |||
| | | | |||||
PACK- | ----------------------------- | -------- | --|--------- | --- | ------------------------- |
--| |
As you can see we have a constant load of around 0,18 mA and for the manual peak we have 3,4 Volts with an combined Resistance of 145,8 Ohm. Which makes around 23 mA. If I calculate the resistance of my LS17500 it's around 8,36 Ohms.
- Put Jumper into the GE-Pull-up
- wait until BQStudio recognises the Board and wait until GA Bit is low
- Gauge Start
- wait a second and wait until GA is high
- Press manual Switch for a second
- release manual Switch and Gauge Stopp at the same time
- wait untill GA Bit is low
- check registers in BQStudio.
Checking the Data Graph with the register voltage and scaled R I see my drop > 100 mV.
There i have the SOH_Merit high, sometimes also the SOH_ERR high. Scaled R is around 3-4 Ohm. If I wait a few moments and do the steps 2-8 again (without pulling/putting the jumper out/in) then I get my Scaled R at around 8 Ohms (which is almost the same as my calculated result) but I still get the SOH_MERIT Error.
Everytime i do the above steps or the second steps without GE-Pull-up my SOH decreases 2 %.
Calibration was made in ACC mode and then changed to EOS Mode.
If I choose a different Lithium Thionyl Chloride Battery, the values in the Table (Data Memory Contents) are changing. So I think I also need the correct Chem ID for my battery to see if my SOH or EOS is calculated correctly.
So what am I doing wrong?
Best regards
Benjamin Meder
-