This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53659: Is SVID rising/falling timing adjustable?

Part Number: TPS53659

Dear Experts,

Is SVID rising/falling timing adjustable?

Our "data" rising is about 608ps and Spec. is below 380ps.

We have tuned SVID pull-up resistor but it will also affect rising/falling timing at the same time, it seem not the best method.

  • Hi Jan,

    SVID is an open drain interface, and the pull-down strength of the buffers in TPS53659 are fixed (not adjustable). The only "knob" available to tune would be the placement and strength of the pullup resistors. 

    You may want to check the bandwidth of your scope/probing also. Example, with 300ps is well outside the bandwidth of a 500MHz scope. 

    Are you actually seeing SVID communication failures?