Dear All:
I use the BQ76940 to design the 16s bms, when I do the OCD testing, I find the the MOS Q38 between the Cell 15 and REGSRC is damage ,as below is schematic, and the DS wave, can you explain what cause
the result. Thanks~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear All:
I use the BQ76940 to design the 16s bms, when I do the OCD testing, I find the the MOS Q38 between the Cell 15 and REGSRC is damage ,as below is schematic, and the DS wave, can you explain what cause
the result. Thanks~
Hi Bill,
I think a diode / resistor pair is needed to protect the FET by reducing the power during a heavy load. Section 9 of this app note discusses this need in much more detail: http://www.ti.com/lit/pdf/slua749
You can also refer to this 15s reference design to see example component values: http://www.ti.com/tool/TIDA-00255
Best regards,
Matt