Part Number: BQ27220
Other Parts Discussed in Thread: GPCCEDV
Hi TI team,
We are using the BQ27220 fuel gauge in our design and as I went through the forum questions I came across an answer concerning changing the design capacity. We want to change the design capacity from the default (3000 mAH) to 9600 mAH and the question was asked do any of the other parameters need to be changed. We are adding two more cells in parallel to increase the capacity.
The response from dMax was "Besides changing Design Capacity, they also need to scale EDV R0 inversely proportional to cell capacity. If they double the cell count then they should halve EDV R0."
1. Would this also be true for the BQ27220?
2. Would I also want to change the default Full Charge Capacity initially?
Respectfully,
Keith Haydon