Part Number: LM3481
Other Parts Discussed in Thread: LM3478, LM3488, LM5155
Hi
I have a system requirement where I need to drive a portable printer from a single cell Li-ion battery (3.6V-4.4V). The printer drives at 12V and has a 3A current requirement.
I was thinking of using a boost controller for this.
However when looking at LM3481 datasheet and also the AN-1756 which is its EVM, they only mention a current < 1.5A. Im not sure why this is? Says that on the very first page of the EVM app note.
If its a boost controller, shouldn't its current output depend on the capability of the external FET. As long as the boost can drive the FET, it should be ok right? Shouldn't I be able to use the EVM to work at 3A output at 12V.
Also, the datasheet for the efficiency curves for LM3481 only have till 1A? Why is that?
I've seen similar parts like LM3478, LM3488, LM5155 but they all have the same confusion.
Hoping someone can clear my confusion or mis-understanding on how the controllers work :)