This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir
I would like to make a transient simulation of the UCC28780 Active Clamp Flyback 45W AC/DC EVM with GaN FET. I see that only Simplis Model of the UCC28780 and UCC24612 are available.
Could you provide the spice model of the UCC28780 and UCC24612 in order to make a LTSPice Simulation or the only way is to do a simulation using Simplis?
Thanks
Best regards,
Nicola
Dear Eric,
thank you for your response!
Could you provide the PCB layout file of the UCC28780EVM-002 for reference (like CAD file)?
I'd like to refer the layout and try to realize the PCB by myself in order to practise.
Thanks
Best regards
Nicola
Nicola
UCC28780EVM-002 was developed in Altium. Attached are the Altium files and gerber files for this design.
Best Regards,
Eric
Dear Eric,
I'm able to open the schematic files from the design files but not the PCB project.
I'm using Altium 2018.
Please let me know
Best regards
Nicola