Hello,
I would like to use LM5176 in a constant current source, for example CC 10A ps.
If I look on internal Functional Block Diagram is output of crrent sense amplifier compare with internal referne 45mV and comparator dischrge external capacitor on SS input.it can be said,
CC control loop switching controler to Soft start , my question is how to correctly choose the size of the starting capacitor on SS input? For example if switching frequency is set on 230kHz