This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61260: Inductor size reduction

Part Number: TPS61260


Hello all, I'm on a new design involving a TPS61260DRVR - 4V output and Iout Max 100mA. Recommended inductor is LQM2HPN4R7MG0 which is quite big 2.5mm x 2 mm (1mm tall). 

I wanted to reduce inductor's size. My candidates are: DFE201610E-4R7M=P2 and LQM18PN4R7MFRL. Are they suitable for this application?

Thanks in advance,

Víctor