This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34110: Learning load parameters

Part Number: BQ34110

We plan to use the bq34110 in a high capacity/ high cell count application: 6...12 NiMH cells/ 6...30Ah. Because the maximum power dissipation of the learning load is limited in this application we are looking for the lowest discharge current usable in the learning phase to 1..2% discharge the battery. In the datasheet I only found C/100...C/10 as a general recommendation, but how to determine the optimum value for a certain battery pack?

Another question I have: because in our application the BMS system has to support several types of battery packs it is necessary to adjust the learning load resistance according to the pack type. Is it possible to do it by using a PWM modulated fixed resistor load?  And if yes, what the optimum PWM frequency range would be?