This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LT1054: positive doubler and inverter

Part Number: LT1054

Can I use the chip to do double from 14 to 24V and -12V using single device?

I see the circuit for positive and negative doubler with one chip in the datasheet, I assume it is probably possible for 2X and -1X with single chip. 

Also, please recommend ways to reduce the ripples.