How do I get this chip BQ24075RGTR out of sleep mode?
Ref datasheet: The datasheet http://www.ti.com/lit/ds/symlink/bq24075.pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
How do I get this chip BQ24075RGTR out of sleep mode?
Ref datasheet: The datasheet http://www.ti.com/lit/ds/symlink/bq24075.pdf
Our power source is a wireless power receiver. It appears that during transient load changes, the input(VIN) to this battery charger IC collapses, causing it to enter sleep as expected. Therefore we suspect this IC puts VBAT (4.16V) on VIN, which appears to contend with the output of the wireless power receiver. This condition persists until the sleep timeout approximately 20mS later when the system restarts. We are hoping to disable sleep mode to test our theory.
The data sheet indicates that after 20mS into entering the sleep mode the FET is disconnected. We are concerned about the 20mS duration behavior.
9.4.1 Sleep Mode
When the input is between UVLO and VIN(DT), the device enters sleep mode. "After entering sleep mode for >20
mS the internal FET connection between the IN and OUT pin is disabled"
Please find a scope shot captured from our test.
Ch1 shows the Vin follows Vbat for 20mS then the FET gets turned off.
Hello,
Can you try this with a lower VBAT(around 3.2V) and post the scope capture. Also try to connect the anode of the diode you have on /PGOOD to SYSOFF so that the connection to the battery is turned off and let me know what happens. This is done to ensure VIN is absent before going into sleep mode.
Thank you so much for your help.
In our design, we are powering this TI part with IDTP9027LP which is a Qi WPT receiver.
The IDT chip has a slow response to transient events.
If you have any suggestion how to hold the VIN to TI part when there is a certain demand of current, it would be helpful.
We are right now using capactiors upto 40uF at the VIn node.
We thank you again for your help.
Thanks,
Priya