Other Parts Discussed in Thread: LM5019, TPS54360
Hi,
Here are some question for previous comment
- "AGND and DGND should be connected together to the ground plane and Vpwr and VDD should be referenced to the same ground."
If I connect PSE_GND and A_DGND with a short pad, is this work? Or I have to use the same GND plane for VDD and VPWR instead of use 2 GND plane and connect them together?
2 The UVLO for VCC_3.3V DCDC is beter to set above TPS23880's UVLO(18.5V)
Refer to TPS23880EVM, the power rail LM5019's enable(19.64V) is above TPS23880's UVLO rising, but disable(10.58) is lower than TPS23880's falling UVLO
Due to the TPS54360's UVLO has no voltage hysteresis, which one should I follow?
Thank you.
C.T.