Part Number: TPS40170
Other Parts Discussed in Thread: LM5146-Q1
Hello everybody,
Our product using TPS40170 failed on EMC radiated test at ~96MHz - so it's definitely common-mode noise problem! We narrowed it down with EMC probes and Spectrum Analyzer and we think the problem lies in buck.
My schematic is:
During PCB layout I paid attention for "power" loop to keep it small as possible. Layout looks like:
I did measurements on some critical points of the system: SW, LDRV, HDRV, OUTPUT node using "short ground probe".
HDRV node:
LDRV node:
SW node:
Output 5V:
Of course, one of the possible solution is to add common-mode clamp on the input, but I would like to mitigate the source as much as I can.