Hi, my customer is using UC2804 as aux power. The schematic is as below.
BUS+ and BUS- are from PV panel. The PV panel's voltage will start rising with light on the panel.
Now when UC2804 start working when PV panel's voltage rises to a level. They will observe it repeatedly start up. But they measured VCC with multimeter, it's always 9.3V. I guess the repeatedly start up is causing by the turn on:12.5V and off:8.3V threshold. So I will ask them to measure VCC through scope.
But the start up repeat frequency is so high that I'm not sure if it's caused by the on and off threshold.
Any other pin's waveform is suggested to measure to determine the root cause?