This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61194: Setting Vout against max LED Vf

Part Number: TPS61194

Hi team,

I used TPS61194 in a previous design, which used an LED string with a max Vf of 30.6V. Per the note in Section 7.3.1, I set my Vout to 1.3 * 30.6V = 39.78V. [Related section: "VOUT_MAX voltage should be chosen based on the maximum voltage required for LED strings. Recommended maximum voltage is about 30% higher than maximum LED string voltage."]

In an upcoming design, the LED string I'm using has a max Vf of 37.4V. Taking the same approach, I should have a Vout of 48.62V, which is too high for the device.

So I have two questions:

  • Am I approaching setting my Vout correctly against my Vf?
  • Given my new Vf, am I correct in assuming I need to find a new device for this project?

Thanks,

Brian Angiel