This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5160A: 5160A diode (DFL1100-7) > 100ºC

Part Number: LM5160A

Hi,

We use LM5160A for flybuck. The input is 9~36VDC and output is 24V. There is a problem is that when the input over 30V, the diode D3 temperature is very high.

Do you have any recommend?

Output: 24V / 35mA

Best Regards,

Aaron