This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/BQ34Z100-G1: regarding reading high current above 10 amp to 100amp using shunt resistor 750 uohm .

Part Number: BQ34Z100-G1
Other Parts Discussed in Thread: BQSTUDIO

Tool/software: WEBENCH® Design Tools

As in the bq34z100-g1 evm board  , shunt resistor is capable  upto 7a current .

so we removed the shunt resistor in evm  and replaced  a local shunt resistor which is capable of high current  with specification of 0.75 m ohm , 7w .

but values are getting undesired values of charging and discharging current in bqstudio .

what are the required settings to be   considered for getting correct values .

'our task is to read the high current through battery from the range of 10 a to 100a .

what are the steps to be considered regarding using above shunt resistor .

why iam unable to read 10 a current in bqstudio?