Other Parts Discussed in Thread: TPS92518
Hi Team,
my customer is interested in the TPS92518HV for a next generation product. They found the note in datasheet section 11.1 to place the output capacitor close to the LED if the LED is not directly at the part. But unfortunately the datasheet does not contain a recommendation which maximum distance should be maintained with TPS92518HV between the part and the LED.
So the customers question is:
1. For the specific project they will have a cable of 50 to 100cm length, is this possible?
2. If yes, which measures should be implemented to achieve best results with such length if possible?
3. If #1 yes, what is the maximum cable length which you have tested in the lab? Which is the longest cable you would still see as possible with TPS92518HV?
Thanks in advance
BR Cevin