This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28064A: Effect of Inductor Accuracy

Part Number: UCC28064A

Hi Team,

 I have question about Effect of Inductor Accuracy.
 The Interleaved PFC is controlled 180deg switching.
 In case of the Inductor accuracy is +/- 10%,
 1. How will it affect the behavior?
 2. Does it affect phase 180 degrees? 

Regards,
Ogasawara

  • Refering to the datasheet, page 15, Section 8.3.2, Natural Interleaving, where it describes the device has mechanism to adjust control to maintian 180-degree phase and tight boost inductor tolerance is not required for 180-degree phase. But inductor tolerance will affect peak current based on Equation (1) on page 16.