Hello guys,
One of my customers is evaluating TPS92515 using TPS92515 EVM (TPS92515HVEVM-749) for their new products.
http://www.tij.co.jp/jp/lit/ug/slvuar5/slvuar5.pdf
In the evaluation, they observed that the output current is unstable (the current change 800mA~1200mA, target is 1000mA) like a oscillation. They use 1meter length wire
(AWG24 or AWG26) between EVM J2 and LED lamp.
They think this length may be too long for TPS92515. In other word, this long wire causes the unstable output current.
Could you give me your answer to the following question.
Q1. What is the maximum wire length between EVM and LED lamp in their test condition?
Their test condition:
Vin=24V, Vout=1 LED (Vf=2.0~2.2V), Iout=600mA~1000mA.
Q2. Is there any way to avoid the output current oscillation?
Your reply would be much appreciated.
Best regards,
Kazuya Nakai.