Other Parts Discussed in Thread: TPS63060
Hi
I am using the TPS63070 IC in one of my design for output of 8 V and Load current of 2A ,
The design is working fine but while checking Load (or) output current with adjustable Resistive Load till 600mA while turning on Power supply is working fine but after that when I am reducing the resistive load for >600mA before turning ON , the current is dropping to 150mA approx. after turning ON supply
In case if I am connecting and adjusting/ varying the load after turning ON power supply then I can measure up to 2A with out any issue , Can you confirm whether it is the limitation of start-up current? Even in datasheet pg 21 shows the typical start-up current limitation for 8V o/p is around 750mA , and I tried by connecting high Value of capacitors at I/p and o/p up to 100uf , however there is no improvement, Can you check and do the needful?
Thanks,
Praveen
Mob:9902401702