Other Parts Discussed in Thread: BQSTUDIO
Hello,
After calibrating my BQ34110 chip and changing data memory values, the chip is now reading current, temperature, and voltage values rather accurately. However, it is continuously showing 0% SoC on the battery gauge icon. While doing 1s calibration the SoC was staying around 95-100%, but when increasing the number of series cells the SoC dropped to 0%. Could someone give advice as to why this is happening and/or how to fix this? Is it a value in the data memory that has been programmed incorrectly? We have not yet done a full discharge cycle, if that's important. We are using a 6 cell, 12 V, 8 Ah, lead-acid battery. I have attached the .gg.csv file (had to convert to a .doc for upload):
Thanks in advance,
Colin