Other Parts Discussed in Thread: TPS709, TPS7A26, TLV767, , LM5118, LM5117
Hello,
I am working on a new design in a highly inductive environment with 48V PWM switching on solenoids. Our limited testing revealed that we have current flowing through the low voltage ground, causing our I2C bus to miss commands. (The current raises the ground high enough that with noise and ground swings we missed some I2C commands) In order to mitigate the problem, we plan to isolate the communications from the rest of the board using an RS485 with opto coupling (ISO308x). I was looking at the datasheet for the UA78M05CDCYR and it looks like it should have enough power to drive the RS485 high side. We plan to have 12V Differential signals and a +12V computer power supply at the input jack to the board.
With that in mind, I think this power regulator should be more than sufficient to power the RS485 chip, is this assumption true?
Also, for reverse voltage protection, I was considering using a schottky diode (ST P/N STPS1L40ZFY) but aren't sure how much negative current the voltage regulator can handle. I chose a schottky diode with a reverse voltage of ~30uA and a foward voltage drop of ~0.25V.
Any recommendations would be greatly appreciate!
Thank you,
Josue Cruz-Lambert