Hi team,
Could you please help to check if we have low IQ LDO, lower than TPS709, with AEC-Q100 qualification? Better to have SOT-23 package. The input voltage is 5V, loading current less than 100mA, adjustable output voltage.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Could you please help to check if we have low IQ LDO, lower than TPS709, with AEC-Q100 qualification? Better to have SOT-23 package. The input voltage is 5V, loading current less than 100mA, adjustable output voltage.
Thanks
Hi Fery,
We currently have 19 automotive qualified LDOs in the SOT-23 package as shown on our product parametric search that can support the input voltage and load current you state. TPS709-Q1 has the lowest Iq of these devices.
Very Respectfully,
Ryan