I have been attempting to validate the BQ24610 charging profile. I was attempting to get a charge current of 2.5A, according to the data sheet that required a ISET1 Voltage of approximately 0.5V.This is based on the equation:
I_CHARGE = VISET1/(20*RSNS)
I attempted to achieve this with a voltage divider consisting 100K Resistor (R1) tied to VREF and an 18K resistor (R2) tied to GND. I am using an RSNS resistor of 10mOhm. I measured the voltage of ISET1 to be 0.48V but were only getting a charge current of 1.5A.
To test our design and check for potential pin assignment issues I added to 100K in parallel to R1. This put the voltage of ISET1 to 1.14V and the charging current closer to what we wanted, at ~2.4A. According to the data sheet, though, I should be seeing a charging current closer to 5A.
I am unsure what the issue as, it appears that the voltage of ISET1 is controlling the charging current but it's not following the equation outlined in the data sheet.