This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27421-G1: bqStudio Support for BQ27421-G1D?

Part Number: BQ27421-G1
Other Parts Discussed in Thread: BQSTUDIO

I am working with the 'D' version of the BQ27421-G1 device and have version 1.3.54.1 of bqStudio Installed.  According to messages presented by this version of bqStudio, it seems that the '-D' version is not supported?  ( I have not had success accessing the 'D' version of the device, but can access 'A' version fine).  Is there another tool available to access the 'D' device?  I see a test version of bqStudio (1.3.86.3), would this support it?  Thanks

  • Hi Christopher,

    Please download the test version. It may have the bqz for the G1D. If not, please reply here and we will provide you with the G1D bqz.
  • Thanks for the response.  I downloaded and installed bqStudio 1.3.86 (Test Version).  This version does NOT automatically detect the 'D' Revision of the BQ27421 Fuel Gauge, and when I select the 'D' Revision from the Gauge menu I still get the warning that it is not supported and may make the device unusable.  However, if I proceed, it does seem that the program can read the Registers and Data Memory, so that part is good.  My question is do I really run a risk of 'bricking' the device with this version of the tool?  If there is an alternate version of bqStudio that may provide a safer / more stable operation, I would be willing to give it a try.  Thanks!  

  • Hi Chris,
    you should be ok using the bqstudio and device.
    thanks
    Onyx