I am designing a 8 cells Lion-Battery manger using 455A chip.
in this design , the target balancing current is greater than 1.25A @ 3.5V battery voltage by using two of 5.6R resistor in parallel.
To do this current, i need a new and powerful MOSFET to handle the current.
is there any information for me of what's the spec of 455A chip EQ channel drive? like what's the current capability, voltage level when turned on?
Or i have to use recommend MOSFET(2V7002K) with 2k of gate resistor and using other devices like a pnp transistor to amplify the balance current?
thanks and best regards,