Team,
could TPS610995 support 400mA at 2.3 V input voltage and 3.6Vout? What efficiency would be achieved?
I looked at the equation in the DS, but from that it seems challenging.
Thanks for your help,
Bart
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Bart::
According to the test we did before in our lab, it seems Vout still in the normal range of the datasheet(3.53V min, 3.67V max, with PWM mode).
And please realize that the test result is related the circuit design and test environment, just for reference.
Iout A | Temp C | Vin V | Vout V | Efficiency |
0.45 | 85.00 | 2.40 | 3.57 | 84.17% |
0.45 | 85.00 | 2.20 | 3.56 | 80.48% |
0.45 | -40.00 | 2.40 | 3.57 | 91.12% |
0.45 | -40.00 | 2.20 | 3.57 | 89.59% |
0.45 | 25.00 | 2.40 | 3.57 | 87.70% |
0.45 | 25.00 | 2.20 | 3.56 | 85.24% |
0.40 | 85.00 | 2.40 | 3.57 | 85.88% |
0.40 | 85.00 | 2.20 | 3.57 | 83.04% |
0.40 | -40.00 | 2.40 | 3.58 | 91.81% |
0.40 | -40.00 | 2.20 | 3.57 | 90.60% |
0.40 | 25.00 | 2.40 | 3.57 | 88.86% |
0.40 | 25.00 | 2.20 | 3.57 | 86.90% |