This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34110: GPC/Characterizing Cells

Part Number: BQ34110
Other Parts Discussed in Thread: GPCCEDV

Hi,

We are currently using a single 12V, 6-cell, lead acid battery to familiarize ourselves with the bq34110 device, but in practice will be using packs of ~15+ batteries. When creating the 6 data logs using the GPC tool, can we use one battery or should the full pack be used? Also, we'll be using the exact same batteries from the same manufacturer, will we need to take multiple logs of different batteries/battery packs and average the results, or is one sufficient?

Thanks,

Jemma