I'm having some stability issues with the TPS92692. My basic design parameters are:
Input voltage: 9-32V
Target switching frequency 500kHz
Output current: 1A
Output voltage: either 4 or 5 LEDs (12-15V)
I'm using the internally generated PWM with the PFET to provide a secondary 50% operating point
I'm also using the IADJ pin to provide a temp sensor feedback
As the system warms, it starts flickering. I think (although am not sure) that it is because of a capacitance shift in the compensation network (if I use an electronics duster to blow on that area of the PCB, the flickering stops).
I've tried a handful of different compensation configurations and values and haven't been able to solve the issue. I'm going to back to the compensation section of the datasheet to try to understand how to better approach this...guess-and-check isn't working too well. I'd really appreciate some guidance.