This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS16630-32EVM: Pins 24 and 19 on TPS16630 RGE

Part Number: TPS16630-32EVM

Hello,

The datasheet calls out pins 1 and 2 as the power input and pins 17 and 18 as the power output.  The EVM schematic shows pin 24 connected to the power input along with pins 1 and 2, and pin 19 connected with pins 17 and 18.  The datasheet calls out pins 19 and 24 as NC.  Which one is correct?  Does it matter?  Are pins 19 and 24 simply floating anyway?  It would be convenient to use them to pick up more copper in the surrounding area.

Thank you,

David