Other Parts Discussed in Thread: LM25007
I have a wired behavior with my LM284x. My circuit should output 5.5V.
If I slowly raise the input voltage Vin from 0...8V the output voltage will raise until 3.28V and stay there. The regulator won't start switching. The same happens if I set my PSU to 8V and enable the PSU because the PSU output raises "slowly" to 8V.
If I set my PSU to 8V and plug in Vin — the regulator will start correctly and Vout is 5.5V.
It seems like the dV/dt has an impact on the function of the regulator. Do you have any idea how to overcome this problem?
ThanksPS: On the Vcc line is a 100u Cap, not visible on this schematic.