This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am using it Full bridge converter configuration. Input dc is 250V to 380V. Output is variable from 0 to 200V. I am observing Only one pulse release in one of the two PWM output's for lower load or low voltage conditions(around below 10% duty cycle). I am doing external PWM compensation. I am using it only for PWM release. I am facing issue when vdc_error goes below ramp valley value(0.7V to 1.25V).Using only it for pulse release. I have attached schematic,