This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61093: Current rating

Part Number: TPS61093
Other Parts Discussed in Thread: TPS61089, , TPS61372, TPS81256, TPS61085

I am looking for a DC\DC regulator with following requirements :-

Vout = +12V, Vin = +5V Iout = 0.5A aprox.

I am looking for the smallest PCB area !

One of the TI Employees suggested the TPS61093 ! However when looked at the data sheet at it stated that :-


"When the output current exceeds the overload limit, the isolation switch of the IC opens up to disconnect the output from the input" where the overload limit (IOL) = 300 mA TYP ? I require a min current of 500mA ? 

If the TPS61093 will not meet this min requirement - can you suggest a different part ?

Thank you 

  • Hi Shmuel,
    The TPS61093 can't support 0.5A output current. I would suggest TPS61089 which is fully integrated device. so the solution size can be reduce.
  • Dear Jasper Li,

    Thanks for your reply !

    Do you have any other solution with a smaller PCB real estate - I don't need the IOUT = 2 A, our requirements are Iout ≥ 0.5A !

    Best regards

    Shmuel
  • Hi Shmuel,
    the TPS61372 is smaller if the BGA is acceptable. other solutions need an external diode which will increase the solution size.
  • Dear Jasper Li,

    Both of these chips their pitch is a little too small for us. We had a recent design with an IC with a pitch of 0.4mm and we had a lot of trouble with the PCB fabrication and solder mask ! I was hoping for a solution with possibly fewer external components what do you suggest ? I don't think we can go below a pitch of 0.5mm ! Also is there no such thing available with the inductor integrated into the IC - it is usually the inductor that takes up all the room ?

    Thanks again

    Shmuel
  • I am replying since Jasper is out. I found one device(TPS81256) which integrated inductors in MicroSiP package, but it seems it doesn't support 10Vout.
    Regards,
    EL
  • Hi Shmuel:
    1. With inductance integrated: I'm sorry that the module with inductance integrated is not suit for 12V/500mA output as Eric mentioned.
    2. With diode integrated: TPS61372 (with BGA package); TPS61089, small size solution.
    3. Diode outside: TPS61085(with VSSOP package, easy for solder mask). And others...
    I thought TPS61089 is suit for your small size needs if you could accept VQFN package.