This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50: bq40z50r1

Part Number: BQ40Z50

Hi,

I want to use bq40z50r1.

The battery Charge current is 100mA, and the discharge current to the load is 100uA.

I want to use the Coulomb Counter to find the SOC of the battery. The questions are:

1- What is the current resolution? can 100uA and 100mA be sensed?

2- In this case what is the value of the sense resistor should be?

3- What is the error of the sensing (in the above case)?

I read the datasheet a few times, and i cant find the answers to these questions...

Thank you very much!