Other Parts Discussed in Thread: BQ34110
Hi,
Our design uses a BQ25606 for charging a Li-ion single cell battery, and a BQ34110 as a battery fuel gauge. The battery connections are +VBAT and -VBAT, and there is a current sense resistor between -VBAT and GND for the fuel gauge.
The BQ34110 requires a calibration during production (voltage offset and current offset/gain). The currently calibration requires a fixed current going through RSENSE, and the voltage calibration requires a fixed voltage at the VBAT pin of the BQ34110, which is shared with the VBAT pin of the BQ25606.
Currently, our plan is to have the USB powering our PCB, but not have a battery connected. This way, the PCB is powered via the BQ25606. We can then use a current sink circuit between +RSENSE and -VBAT for the current calibration. However, the voltage calibration requires a fixed voltage at +VBAT. We observe that +VBAT is unstable when USB is connected while there is no battery due to the BQ25606. Our question is: can we connect a 4.2V LDO to +VBAT to fix the voltage? Would the BQ25606 detect that the voltage is high enough that the charging can stop?
Thank you,
Fred