Other Parts Discussed in Thread: CSD25402Q3A, TINA-TI, CSD17578Q3A
I am using the CSD17308Q3 in nine places of a design. The idea is to control the VGS of each of these CSD17308Q3 with independent isolated DC-DC converters (that put out 9V for minimum Rds-ON). I have noticed that many of these floating in-line NFETs have a stranger SCR behavior, depending on the load current. I tried to patch the design with increasing the passive resistance between the gate and source. That worked (using external Rgs of 500 ohms, for 1.5A output load), until I needed to bump up the load current some more (about 3 to 5 amps). Now it seems no combination of external Rgs is getting this CSD17308Q3 to turn off when the output load is 3 amps or more. Is there any alternative power NFETs of the same package (the 3.3mm square) that I can replace the CSD17308Q3 with? Any other tricks, to get this CSD17308Q3 to stop behaving like a silicon-controlled rectifier (SCR)? I noticed that while it refuses to turn off (Vgs ~ 0V), once I turn off the drain voltage source, then turn it back on, the CSD17308Q3 then properly stays off. But if it is conducting at 3A or more, I cannot get it to turn off (turning off the drain voltage is cheating). Please help!