Tool/software: WEBENCH® Design Tools
Hello,
I am designing a boost converter to take 42v IN to 90v OUT @ 5A. I used both WEBENCH and the application notes from the datasheet and I'm having trouble with some components.
1) Rsns value is different between the calculation and WEBENCH. If I do the calculation with the components following the application notes, I get a shunt resistor value (Rsns) of 24mOhm and WEBENCH gives me a 10mOhm shunt. which one is correct?
2) If I calculate the values of the whole circuit using the application notes, the values are very different overall from the WEBENCH Design. Which one should I take in consideration?
3) If I want to change the current output of my design in WEBENCH I get a limit of 7A maximum, according to the tool I should be able to get 20A top. Why is this?
4) I tried to simulate the typical application note found in the datasheet that has a frequency of operation of 500khz, but the tool is limiting the frequency to 350khz. I wanted to make the same circuit in order to make comparisons of the applications to see if WEBENCH tool is giving me the close values to the ones calculated in the application note.
Thank you very much for your help!
Kind regards,
Joel