Hi Team
I have aqestion about LM2765.
It is used in the circuit diagram shown in the figure below.
The PWM signal is input to the SD terminal.
When the ambient temperature is raised,
The VOUT rises linearly at 80 ° C ambient temperature when the SD pin is high.
It increases to the maximum rating. After that the output drops.
Have you ever had such a phenomenon?
I do not know the cause, please support.
Best Regards,
Ishiwata