This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61028: VBAT / GND Short

Part Number: TPS61028


Hi,

We experience the problem that the TPS61028 fails under unknown circumstances. 

What happens is the part develops a short between VBAT and GND, 

  • The layout is as recommended in the datasheet
  • Instead of a tantalum C we use a ceramic C plus series resistor
  • On the input side we never observe any voltages greater than 5.5V
  • The component is not exposed to hot environment
  • In our lab we cannot reproduce the fault (e.g. with excessive input voltage, noise, short on output, ...)
  • We use EN to infrequently start/stop the converter
  • We boost from Li-Ion cell to 4.2V
  • We operate the part in continuous mode (i.e. PS pulled high)

Any help is greatly appreciated

Matthias