The electrical characteristics page of the datasheet specifies typ. 3.2V, max 3.8V oscillator sync threshold, while chapter 8.2.2.4 states that the sync signal must have an amplitude between 1.5V and 3.0V. Does these two statements mean different things or is one of the statements wrong? I guess I will eventually figure out how this works, but it would be nice to know beforehand.