This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR36015: UVLO setting and hysteresis value

Expert 4640 points
Part Number: LMR36015

Dear e2e Support,

In our datasheet, we are showing our typical value for the hysteresis Ven_Vout_hys (110mVtyp).

Can we provide any min/max data?

Is it guaranty/qualified from -40° to 85°C?

My customer intend to use a 820K/100K resistor bridge to get the following voltage value:

Min

typ

Max

Start

10,645688

11,3252

12,004712

Stop

9,633688

10,3132

10,992712

Regards,