Other Parts Discussed in Thread: LM5155
Hi all
I have this question for the LM3481:
- For parameter Vsense, current sense threshold voltage, the typical value at 25°C is 160mV.
What is the expected tolerance of this parameter independent of temperature? - Over the operating temperature range of -40°C to 125°C, Vsense can vary from 100mV to 190mV. What is the numerical sign of the temperature coefficient? Does Vsense increase with temperature?
I am looking forward to your feedback.
Best regards
Ueli