Other Parts Discussed in Thread: TPS62651, TPS62750, TPS61088, LM27762, TPS61041
Dear Ti support,
I am performing test with the TPS62751 Step-Down converter.
My requirement are:
- input voltage from USB-C (from a tablet): 5V (can go as low as 4V when drawing 1.2A)
- output voltage 3.7V
- output current target 1A.
I performed my test on a dedicated layout (see schematic below), Rlim High is 20k which should limit the input current to ~1.23A. My observation is that the output voltage drops well before reaching the input current limit as shown on the graphic attached. Blue, Grey and Yellow curve are done with a lab 5V supply. Blue curve corresponds to the schematics, the Grey curve has an increase Cout (+ 3 cap ceramic X7R of 10uF), the Yellow has a increase inductor (3u3 with smaller R). This changes tends to improve the perforamance at higher load.
Then I powered the device with the tablet. The RED curve shows the performance with the tablet. The tablet voltage is reduced depending on the load (pink curve, right axis). and the ouptut voltage is not really regulated to 3V7 as we can see on the RED curve. (this measurement were done with the improved circuit , corresponding to the Yellow curve when powered with a regulated 5V input voltage).
Any recommendation to improve this circuit. I am hesitating to order the EVM to check if I get the same results, but maybe you can already inform me about some limitation of this circuit.
It seems that the datasheet figures are done with limitation near 700 mA (R_lim_U ~50kOhms), is this correct, I cannot find this information in the datasheet.
thanks for your help.