This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

+12V \ -12V Power supply

Other Parts Discussed in Thread: TPS65131

In my design I need 2 supply rails +12V & -12V from a +5V. I will be using these supplies to power transceivers that are rated a max current drawn of 120mA\130mA. In order to give enough spare in the power ratings of the required solution I thought of looking for DC\DC that would provide 0.5A max (maybe this is over kill ???). We are concerned about the heat and limited space requirements of our design. I found the LT8335 (Typical application : 5V to 12V Input, –12V Inverting Converter) and the LT3580(Typical application : 2MHz Inverting Converter Generates –12V from a 5V to 12V Input) and now comparing them as well as potential options of other suppliers solution. 

Does TI have anything that can provide a better solution ?