Hi All!
Our application requires a buck/boost IC that puts out 5V from a 3.7v Li-Po battery pack, which get charged by a USB connection which might be higher than 5V.
We currently use the TPS73733 which puts out 3.3v, when the input voltage is between 2.7V and 6.0v. This works perfectly!
I there a similar device from TI that can take 2.7V to 6V in (or close to that), and put out 5.0V in a buck/boost fashion (if the input V is either higher or lower than 5V?
(Sorry for reposting this...my previous question was closed for some reason.)
Thanks!