Dear friends,
i want to power up my cc3220 customized board through 10W solar panel with out battery.
so anyone can suggest best power regulator for my need.
thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Natesh,
It seems as though there will be a variable input voltage for this application. Can you please confirm what the range is for this as well as the expected output current? Do you need a device to just power the CC3220 or will this be used to power something else as well?
I would like to recommend you use a buck/boost in front of an LDO regulator. Some devices that I can recommend for the LDO would be: TLV767, or TPS7A26, TPS709 if low ground current is needed.
You may be able to get more ideas on how power supplies are done by checking out the Solar energy section of the Grid Infrastructure landing page: 
Regards,
Wilson
Natesh,
You can check BQ24650, a battery charger with input voltage dynamic power management for solar panel applications www.ti.com/.../BQ24650.