This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC59108: Dimming issue

Part Number: TLC59108


Hi

Problems are occurring at customers.

The customer concurrently controls OUT 0 to OUT 7 using the GRPPWM register of TLC 59108.
The duty of GRPPWM is controlled from the host to the TLC59108 at intervals of 5ms.
However, duty is not reflected at a fixed timing, resulting in the LED being stopped, causing the LEDs to flicker.
Is there anything you can think about this cause?

TLC59108.pdf

Best Regard

T Kishi